TI E2E Community (Beta)
Welcome to the TI E2E (Engineer-to-Engineer) Community! We invite you to freely and openly interact with your peer Engineers, TI Engineers, and other experts in order to ask questions, share knowledge, explore ideas, and help solve problems.
More Search Options

Local variable placement on stack or not

rated by 0 users
Not Answered This post has 0 verified answers | 1 Reply | 2 Followers

Not Ranked
6 Posts
Community Member
Cool Javelin posted on 3 Nov 2009 6:24 PM

I have noted that the C compiler may place some local variables in the .bss section rather then allocate them on the local page frame.

Using CCS DSK 2.21, and the C2000 compiler for the 2407A processor.

If I make a small function, like:

int DoSomething(int a, int b)

{

int c;

  c = a + b;

  return c;

}

then a and b get pushed on the stack by the calling function and c gets allocated to the local page frame and accessed via reg A0 as expected.

---

But, if I allocate many variables inside the function, or maybe floating point variables or longint vars, then I note these get put in the .bss section not the local page frame.

Can someone tell me the algorithm CCS uses to determine which ones get placed in the .bss section, and is there any way I can take control of them and force them to be on the local page frame?

---

There was a time I had a stack overflow issue, and I deliberately placed several variables in the .bss section (had to make them global, but accepted that) to reduce the local stack usage.

But, the compiler created it's own intermediate variables and added them to the .bss section too.

An expression like y = (m * x) + b; for example creates an intermediate variable for the m * x result, and another for the addition of the b. Those intermediate results seems to go into .bss section. Can I make them go on the stack?

Thanks for your help,

Mark.

 

 

All Replies

Not Ranked
13 Posts
Texas Instruments Employee

The compiler allocates "static storage duration" variables (globals, and locals declared "static") to ".bss".  It should not allocate non-static locals or intermediate expressions to ".bss".   It may allocate constant initializers for local variables to ".const".  Do you have a test case which demonstrates this problem?  Be sure to include the options used.  Use the "--keep_asm" option and examine the compiler's assembly output; it should be clear which section each variable is allocated to. 

Page 1 of 1 (2 items) |

ALL CONTENT AND MATERIALS ON THIS SITE ARE PROVIDED "AS IS". TI AND ITS RESPECTIVE SUPPLIERS MAKE NO REPRESENTATIONS ABOUT THE SUITABILITY OF THESE MATERIALS FOR ANY PURPOSE AND DISCLAIM ALL WARRANTIES AND CONDITIONS WITH REGARD TO THESE MATERIALS, INCLUDING BUT NOT LIMITED TO, ALL IMPLIED WARRANTIES AND CONDITIONS OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, TITLE AND NON-INFRINGEMENT OF ANY THIRD PARTY INTELLECTUAL PROPERTY RIGHT. NO LICENSE, EITHER EXPRESS OR IMPLIED, BY ESTOPPEL OR OTHERWISE, IS GRANTED BY TI. USE OF THE INFORMATION ON THIS SITE MAY REQUIRE A LICENSE FROM A THIRD PARTY, OR A LICENSE FROM TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI and its suppliers reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.