On the first page of http://focus.ti.com/lit/ds/symlink/pca9545a.pdf it's stated that the device can be used for 1.8V operation. Through out the rest of the datasheet 1.8V isn't mentioned, and it seems, that it mainly focuses at 2.5V, 3.3V and 5.0V operation.
Secondly it's stated that a logic high is detected at 0.7* VCC (page 10). With only one VCC (=3V3?) available (pin 20), is it then possible combining I2C busses at both 1.8V, 3.3V and 5.0V with this device at one time? I think this is unclear from the datasheet. I would like to achive
I2C=1V8 I2C1=3V3 I2C2=1V8 I2C3=5V0 I2C4 not used
Is this possible with this device or would you recommend me doing something else?
Best regards and thanks in advance
Søren
Søren Steen Christensen - SSC Solutions ApS - Web: www.ssc-solutions.dk
The VCC operating voltage is from 2.3V to 5.5V.
However the switches themselves can handle 1.8V to 5V translation. The level shifting is only done with the assistance of external pull ups.
Hi Roland,
Thanks for the answer. This was my understanding as well until I hit figure 3 in the datasheet. This more or less implies, that you need to run the chip at 2.3V - 2.5V VCC in case you want to use it with 1.8V logic, since it's only in this case the chip ensures not to make the 1.8V I2C bus higher than the 1.8V from the pull-ups. - Right? In case running the chip at 3.3V minimum garanteed I2C voltage is ~2.7V - Correct?
Since I don't have any 2.3V (nor 2.5V) supply in my system, I plan to use a level shifter (txs0102 - http://focus.ti.com/docs/prod/folders/print/txs0102.html) for converting my 1V8 I2C bus to a 3V3 I2C bus. Do you see any problems with this approach?
And a second question: Do you see any problems in cascading two PCA9545A chips (one PCA9545A chip connected to one of the 4 outputs of the first PCA9545A chip - Of cause the chips should be configures for different I2C addresses). For some of the other chips (like PCA9515A) I know it's problematic to connect the chips in serie due to the directions sensing method. (See i.e. the thread at: http://e2e.ti.com/forums/t/8919.aspx). I can't find any warnings like this for the txs0102 and the PCA9545A chips, but would anyway like to ask if you foresee any problems using any combinations of these two chips? I.e.:1) Two txs0102 in series2) two PCA9545A in series3) a txs0102 after/before a PCA9545A
Best regards and thanks again - It's highly appreciated Søren
Well, usually for these I2C open drain translation we recommend using the PCA9306.
1) Two txs0102 in series, do see a problem. But not quite sure why you would want to do this.
2) Should be okay. But remember. These are switches, so you need to consider the RON of the device, typically 9-16 ohms depending on the VCC.
3) Should be okay as well, but would like to understand why.
Thanks for your answers and sorry for not being able to get back to you prior to now, but the last week has been pretty tough.
1 & 3) In order to follow up on the thread I'll try to describe my system as I had it while posting the question. It consisted of an OMAP3 (running I2C at 1V8), a lot of I2C peripherals (30+ devices on the 4 paths after the I2C mux) running at 3V3, except for one single I2C device which was running at 5V0.
In order to interface the OMAP3 to the mux I would need to put a level converter between the OMAP3 and the mux (or run the mux at 2V5 in order to ensure 1V8 operation of the mux). In order to interface the mux to the 5V0 I2C device I would need another level converter, since I needed the 5V0 device to be on an I2C path from the mux together with some 3V3 devices. This was my main reason for asking about having two txs0102 in series with a pca9545a in between.
In the mean time I however managed to find a 3V3 compatible part for my single 5V0 device => I don't any longer have the problem.
2) With respec to the RON for the switches in the PCA9545A I think I have accounted for them, but thanks for reminding me in case I hadn't...
Best regards and thanks for your fast and helpful support Søren
ALL CONTENT AND MATERIALS ON THIS SITE ARE PROVIDED "AS IS". TI AND ITS RESPECTIVE SUPPLIERS MAKE NO REPRESENTATIONS ABOUT THE SUITABILITY OF THESE MATERIALS FOR ANY PURPOSE AND DISCLAIM ALL WARRANTIES AND CONDITIONS WITH REGARD TO THESE MATERIALS, INCLUDING BUT NOT LIMITED TO, ALL IMPLIED WARRANTIES AND CONDITIONS OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, TITLE AND NON-INFRINGEMENT OF ANY THIRD PARTY INTELLECTUAL PROPERTY RIGHT. NO LICENSE, EITHER EXPRESS OR IMPLIED, BY ESTOPPEL OR OTHERWISE, IS GRANTED BY TI. USE OF THE INFORMATION ON THIS SITE MAY REQUIRE A LICENSE FROM A THIRD PARTY, OR A LICENSE FROM TI.
Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI and its suppliers reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.