Answer Question #4 - E2E Challenge





Learn E2E

Learn E2E

Learn E2E

The central location for E2E training, feature updates, member feedback and site support

Answer Question #4 - E2E Challenge

  • Comments 14

E2E Challengers post your answer to question 4 below in the comments section. 

(don't worry your answer won't show until after the contest is over!) 

 If you have no idea what I'm talking about check out the rules to play here!

  • 1/3

  • a = (1/y) is the only real number solution. I believe y=63, so 1/63

  • Using the units digit of the decimal equivalent of today’s date in binary as y; which real numbers, a, does the following equation have a unique solution?

    a yx + y-x = y

    a*3 = 1

    so a = 1/3

  • a = (1/3)

  • a = 1/3

  • y=1

    a=1

  • Posted before completing,

    y=1,

    equation becomes, (ay-1)x=0

    solving, equation will have a unique solution for all real numbers where a IS NOT EQUAL to 1.

  • All numbers except 1/3.

  • 1/3

  • Today’s (yesterday's) date is 11/11/11, which is 00111111b as binary.

    This equivalent of 0x3F hexadecimal and 63 decimal.

    Therefore, digits of value of 63 are 6 and 3.

    So, the finally equation is:

    a 63 + 6 - 3 = 6 (or 63a + 6 - 3 = 6)

    And it has unique solution:

    a = 3/63, which is finally:

    a = 1/21

  • 0

  • a=1/63... ( x(63a-1)=0 since 0b111111 = 63)

  • Decimal equivalent of the date "11/11/11" = 63

    Units digit of 63 = 3

    3x + 3-x = y

    Solution: x = 0

  • a=1/63