Hello,
Can I replace the default 1GB DDR2 memory with 4 or 8 GB memory module to allow more samples to be stored?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can I replace the default 1GB DDR2 memory with 4 or 8 GB memory module to allow more samples to be stored?
Thanks.
Igor,
The data transfer speed limitation is the implementation of the USB interface from the TSW1400 to the PC. This is implemented using a SPI type interface to transfer data from the FPGA memory to the PC through the USB SPI interface (slow).
For a faster interface I would recommend designing new firmware for the FPGA to implement a faster/dedicated memory transfer using true USB 2.0 and software optimized for your purposes. You can reuse the same TSW1400 and ADC EVM hardware.
Ken.