Adding files to posts makes the editor unusable

When adding a file to a post I get a ridiculously big image. It covers my whole editor field. This has been there for a long time.

Browser: Chrome 61 on Windows 7.

Also: Which JIRA project can I file such bugs in order to monitor the progress?

Best regards

Richard

  • Thanks, this is a known problem and a resolution is being worked on. There is no JIRA ticket, as it is a ticket with Telligent.

    Bill Traynor
    E2E SysAdmin/DevOps

  • HI Richard,

    A quick workaround for this problem I've found is to:

    1. Click the paperclip icon to attach a file.
    2. Choose your file and hit insert.
    3. Right click on the giant icon and select Edit Media.
    4. For dimensions, enter 75x75 (or 25x25 for a really small icon) and click insert.
    5. The icon should resize.

    Similarly, you can use the Insert/Edit Media button instead of the paperclip button. Using that, you can enter the 75x75 (or 25x25) dimensions right away and not have to edit the huge icon.

    Thanks
    Bill

    Bill Traynor
    E2E SysAdmin/DevOps

Related