E2E Help Central

E2E Help Central

E2E Help Central
The central location for E2E training, feature updates, member feedback and site support

07) Becoming Recognized

Rate This

The Reward & Recognition Program is a way to recognize each member’s contributions to the TI E2E Community. There are numerous ways in which people can contribute to the community, including: asking and answering questions, verifying answers and rating community content, connecting with fellow engineers and adding new content, among others. Each contribution to the TI E2E Community is rewarded with a designated point value.

Explanation of Levels

  Level Member Points Employee Points
Prodigy Prodigy 1 – 250 1 – 750
Intellectual Intellectual 251 – 1000 751 – 3000
Expert Expert 1001 – 3000 3001 – 9000
Genius Genius 3001 – 6000 9001 – 18000
Mastermind Mastermind 6001 – 10,000 18001 – 49999
Guru Guru 10,000 + 50,000 +

 

How to Earn Points

The program is very simple. Various activities on the site have points associated with them, and when a community member does that activity he or she will receive that many points. Specifically, here’s the current set of activities and points for each community activity:

Forums Points
Post Amount each forum post/reply will be worth 10
Reply
Amount each forum reply will be worth 10
Verified answer Amount a user will receive for having a reply verified as the answer
20
Ratings Amount each rating will be worth for original forum post 5
Favorite (user) friend Amount each user will receive for being selected as a friend 5
Blogs
New blog post Amount of points a user receives for making a new blog post 10
Blog comment Amount of points a user receives for adding comments to a blog post 10
Wikis
Wiki comments Amount of points a user receives for adding comments to a wiki article 5
Wiki edits Amount of points a user receives for editing a page in the wiki 10
New design note Amount of points a user receives for publishing a new page to the wiki 20

 

FAQs

  1. Do I start with any points?
    • As many members have already made valuable contributions to the TI E2E Community, we have ensured that all current point levels will be equally recognized in the new point structure.
  2. What level will I start out at?
    • If you are an existing community member your level will be determined by your current number of points. If you are new member to the TI E2E Community you will start out at the “Prodigy” level.
  3. What do the different levels represent i.e. Prodigy, Expert, Mastermind?
    • The levels within the TI E2E Community are used to represent community participation. Identifying top community contributors will allow users to further validate the information that they are analyzing.
  4. How did you choose the names of the different levels?
    • As we at TI identify engineers by their high level of intellectual power, we wanted to ensure that even new community members are being recognized through their knowledge and expertise.
  5. Will there be rewards distributed for top community members?
    • Yes. The rewards system is still in development, but in the near future community members will be not only recognized, but also rewarded for their participation.
  6. What is a rating?
    • Ratings are used to indicate the “usefulness” or “likeness” that community members find in a specific forum or blog post.
  7. What is a verified answer?
    • A verified answer is a question that has been determined as “answered” or “resolved”. Verified answers can be selected by any community member. Questions may have multiple verified answers, however no points will be awarded if the original person to ask a question answers their own question.
  8. Won’t some people try to manipulate the system?
    • Yes, and when we determine that is occurring we reserve the right to either deduct points or remove the users account entirely.
  9. Can I lose points?
    • Yes. If one of your posts is marked as a verified answer but later unmarked, you will lose the 20 points.
  10. Will you be expanding the set of activities that points can be earned from?
    • Yes. Over time we expect to expand this list of activities.
  11. Where can I see who are the experts on the site?
    • Visit the Top Contributors Page.
  12. Why are there points for adding a new blog post, when I can’t even add a new blog post?
    • The ability to add new blog posts are permitted to blog owners only. Currently all blog owners are TI employees. However, we do plan to allow members of the TI E2E Community to add their own unique blog posts in the future.
  13. Do I ever get any actually physical rewards for my participation within the TI E2E Community?
    • Yes! The activity points and community levels portion of the Reward & Recognition Program is only the first phase of the project. Throughout this year we will be adding physical “Rewards” to the program, allowing top community participants to receive tangible items for their valued contributions.

Can’t find an answer to your question? Please post your question here.

Comments
  • How do you track Wiki edits in e2e account? Are Wiki and e2e accounts connected?

  • Hi Constantine,

    The wiki pages, edits and comments are referring to activities performed within the "Design Notes" section of each Forum Group. The system does not currently track wiki edits from any external TI wikis, but it is being considered to add that feature in the future.

    I hope this answers your question. Thanks!

    AF

  • Hello,

      I assume that edits to your wiki site http://processors.wiki.ti.com are tracked too, correct?

    --Derek

  • Hi Derek,

    Unfortunately, no they are not...at least not yet anyway. You can find more on this discussion in the comments section of the Ti.com Blog - e2e.ti.com/.../ti-e2e-community-launches-new-reward-amp-recognition-program.aspx

  • I wonder aht the "physical rewards" will be??

  • How do I validate a response?

  • @Chatto...by clicking the "verify answer" button.  If you post a question once its answered we ask that you verify it.

  • How do you add a blog?

  • @Andrew....only TIers can create blogs at this time

  • The points system requires a revision to encourage quality postings. There are postings "How to install ccs3.3" or "how to compile a c program" and "Reporting a bug in assembler / Compiler / hardware behaviour". If all these posting get the same 10 points, the most naive user will become expert!

    I think a community member locating a bug/missing feature and duly acknowledged by TI should be rewarded 100 points. Correct?

    Sayee

  • 2 years ago I started a project in a company which used a TI processor. During my working period I got more than 800 points on the E2E. Later the company split so my mail was changed and I was forced to start a new E2E account losing all my previous points.

    Now I have around 250 points.

    Can the points I earned before be added to my current points?

  • @Nir  - Yes we can combine your accounts.  Private message me with a link to your old profile page and a link to your new profile page and I will join the two accounts together

  • This is a cool concept

  • @Andy Justice:

    When I became guru right after the program was introduced, I got a $100 code for the TI shop. When being elected for the contributor of the year 2010, I got a lifetime free code for MSP tools as well as an invitation to the 2011 ATC (which was cancelled). This was officially announced in the MSP forum.

    @Mokan Kanna:

    Indeed, posts like " I'm paid for a project, can you writ eme the code for free? " shouldn't get any points.

    Also, some clever people verify their own 'thanks for the answer' post. Surely not the intention of the inventor. However, I'm in the lucky position to look at this veeeery relaxed. :)

    @Foe/Nir Aloni:

    Can't you change yourmail address in the profile page? Oh, I see, you cannot, the field is read-only. The question is: why?

  • @Jens Michael - E2E using the my.TI login.  Any changes to email should be done by logging into the my.TI login at the top of the TI header, from there on the my.TI homepage you can change all your contact information and preferences.