Stellaris Launchpad Data Logger v1.0 (Fixed)

PROJECT DESCRIPTION (GUI & Codes Updated: See "User Guide" Section)

The main aim of the project was to create a Simple, Easy to control Graphic User Interface (GUI) to display, plot and log the data obtained from the ADC pins as well as the Internal Temperature Sensor of the Stellaris Launchpad via a H/W UART Interface. The GUI for this purpose was created using Visual C# and can be used on any Windows based PC/Laptop. The newer version of the GUI also allows the user to control Port B Pins (Switch ON/OFF) of the Stellaris Launchpad.

Project in Action

                        Fig: Graphic User Interface (GUI) of the Project (Updated)

GUI FEATURES:

  • Obtain & Display data obtained from the ADC pins of the launchpad easily.
  • Data obtained can be plotted realtime & Graphs can be saved in standard image formats.
  • Data can also be logged into an excel file and saved for further use.
  • Toggle On Board LED(s) (Just for fun !)
  • Toggle Port B Pins on the Stellaris Launchpad