Browse by Tags
Microcontroller Projects
blank
Join group
Get this RSS feed
Tags
430
android
Battery
bluetooth
Booster Pack
capacitive touch
clock
controller
Co-op design challenge
LCD
LED
matrix
motor control
MSP
msp430
MSP430 Launchpad
MSP430G2452
msp430g2553
music
piezo
RGB
RGB LED
robot
sensors
Servo
Related Posts
File:
A Weekly Thermostat with the MSP430
Ruffin White-Magner
PROJECT NAME: My MSP430 LaunchPad Project TEAM MEMBERS: Ruffin White Michael Yuhas Video Link: http://youtu.be/0rrDt5NaOX8 PROJECT DESCRIPTION Normal 0 false false false EN-US X-NONE X-NONE ...
on
Jul 29, 2011
File:
Audio Input / Output Switchbox
Evan Cornell
Audio Input / Output Switchbox TEAM MEMBERS Evan Cornell (corneled@rose-hulman.edu) PROJECT DESCRIPTION This project utilizes the MSP430 to switch between several audio input and output options. The purpose of this project is to be able to choose an audio source...
on
Jul 27, 2011
File:
Bike Computer
ANDRES RADA
MSP430 LaunchPad Bike Computer TEAM MEMBERS: Andres Rada PROJECT DESCRIPTION A bike computer is a device mounted on a bicycle that calculates and displays trip information, similar to the instruments in the dashboard of a car. The computer with display, or head unit, usually is attached...
on
Jun 20, 2011
File:
CardioDroid - Connecting TI and Android
Daniel Ogilvie
CardioDroid Connecting TI and Android TEAM MEMBERS: Daniel Ogilvie, Junior, University of Texas at Austin Michael Sherman, Sophomore, University of Texas at Dallas Blessing Oskaue, Freshman, University of Texas at Dallas Voting is now open! Vote HERE for CardioDroid ...
on
Jul 28, 2011
File:
embedXcode — Use Xcode to develop for LaunchPad platform!
Rei VILO
Use Xcode to develop for LaunchPad platform! embedXcode is a full Xcode 4 template. Thanks to its modular structure, embedXcode can implement virtually all Processing-based IDEs and platforms. It relies on Energia Arduino-based IDE and currently supports the MSP430G2xxx , MSP430FR5739 and Stellaris...
on
Apr 7, 2012
File:
G3TR for MSP430 LaunchPad
giuseppe talarico
G3TR means: Giuseppe Talarico Transistor Type Recognizer. The required additional hardware is very simple: just two 10K resistors. A serial Terminal ( PC or LCD ) is required to show the test result. It allows to recognize the type of a transistor. The transistor that can be tested are: pnp or npn...
on
May 20, 2011
File:
Interfacing LaunchPad to digital caliper
AdrianFer
This project shows how to use the LaunchPad to send readings from a digital caliper to your PC using an RS232 serial port. Check out robocombo's blog for a complete write up, source code, schematics, images, and other resources! http://robocombo.blogspot.com/2010/12/using-tis-launchpad-to-interface...
on
Apr 18, 2011
File:
Interfacing LaunchPad to TLV5620 (4ch DAC) for waveform generation
AdrianFer
This project shows how to interface the LaunchPad to TI's TLV5620, a 4 channel 8-bit Digital to Analog Converter (DAC). Please visit Suspended-Chord's blog to find pin connections and a code library for interfacing with the DAC. http://blog.suspended-chord.info/?c=9
on
Apr 18, 2011
File:
LaunchPad + Sparkfun LCD: Button press counter
AdrianFer
This project shows how to interface a serial communication between the LaunchPad and an LCD from sparkfun. This project shows uses an LCD to display a counter signifying how many times the on-board switch on the LaunchPad has been pressed. LCD used in this video: Serial-enabled 16x2 LCD ( sku: LCD...
on
Apr 18, 2011
File:
LaunchPad and piezo speaker playing Imperial March
AdrianFer
This project uses the MSP430's PWM output to create simple notes on a piezo speaker. Check out egarante's website for source code, schematics, and more information! http://www.egarante.net/2010/07/imperial-march-on-ti-launhpad.html
on
Apr 18, 2011
File:
LaunchPad Bluetooth Light Controller
Zahid Haq
PROJECT NAME: LaunchPad Bluetooth Light Controller TEAM MEMBERS: Zahidul Haq PROJECT DESCRIPTION Controls a light bulb wirelessly using MSP430 Bluetooth platform + LaunchPad + Capacitive Touch Pad. The overlying goal was to control simple household appliances wirelessly. This not only solves...
on
Jul 28, 2011
File:
Launchpad interface with GSM Modem
RAJESH SHANMUGAM
In This project we are using MSP430 launchpad kit and GSM modem. Based on The Messages PW1/PW2/PW3 the RGB LED will glow in different Color. For demo
on
Nov 19, 2012
File:
LaunchPad interfacing with 2 servos
AdrianFer
This project shows 2 servos being controlled using the LaunchPad. Source code is located here: http://pastebin.com/1Qmkq4a7
on
Apr 18, 2011
File:
LaunchPad Learner
Rachel Quinn
See also: n-back Research Video -- University of Michigan researchers discuss their findings on a study of the benefits of n-back. BY: John Hermiz [j-hermiz@ti.com] Rachel Quinn [rachel.quinn@ti.com] Daniel Schucker [d-schucker@ti.com] ...
on
Jul 28, 2011
File:
LaunchPad metronome with MSPGCC
AdrianFer
This project shows users how to create a simple metronome using the LaunchPad's on-board LEDs. The project was created using MSPGCC, an open source IDE alternative. Checkout Joby's blog for source code, schematics, and additional info! http://blog.hodgepig.org/2010/09/08/571/ [Video]
on
Apr 18, 2011
File:
LaunchPad morse code beacon
AdrianFer
This project uses the LaunchPad to send out morse code messages using an LED. Source code is available by lastaid at http://pastebin.com/XSyAN6x5
on
Apr 18, 2011
File:
LaunchPad morse code transmitter
AdrianFer
This project is a LaunchPad-based morse code transmitter. It can translate characters sent through the COM port from the PC into morse code. Additionally, users can send out morse code using a key switch. Check out ech0s instructable here: http://www.instructables.com/id/LaunchPad-Serial-Morse-Transmitter...
on
Apr 18, 2011
File:
LaunchPad theramin, interfaced with photoresistor, potentiometer and speakers
AdrianFer
This project creates an audio modulator using the LaunchPad, photoresistor (CdS cell), a few potentiometers, and a piezo speaker! Visit Suspended-Chord's blog for code, images, and even an audio sound byte! http://blog.suspended-chord.info/?c=17
on
Apr 18, 2011
File:
LaunchPad voltmeter
AdrianFer
This project uses the LaunchPad to create a simple voltmeter, which sends voltage data to your PC's hyperterminal! Visit Frank's blog for a complete write up, source code, screenshots, and other resources! Note that the blog post is in German. http://www.frank-buss.de/LaunchPad/index.html For...
on
Apr 18, 2011
File:
LaunchPad with light sensor and bluetooth (BlueSMiRF)
AdrianFer
This cool project uses the LaunchPad to answer an age-old question - Does your refrigerator's light actually turn off when you close the door? Check out Mike's post at his blog for a nice write up, schematics, code, and more information! http://grieg.gotdns.com/blog/?p=215
on
Apr 18, 2011
File:
LED Matrix Interactive Periodic Table (New Content)
Austin Beam
PROJECT NAME: LED Matrix Interactive Periodic Table VOTING: If you like what we've done and you are a TIer, we would love your vote in the TI co-op challenge! You can vote here. Thanks for your support! VIDEO DEMONSTRATIONS: Unfortunately, neither regular HTML nor the method suggested...
on
Jul 29, 2011
File:
LightPad (Mobile Light Effects Controller)
Aldo Briano
Project Members: Aldo Briano Stanford University (abriano@stanford.edu) Overview LightPad lights up a room to the creativity of its user and the rhythm of the music. It is an Android hardware accessory that communicates wirelessly to the phone. LightPad's intuitive interface...
on
Jul 27, 2011
File:
miniSUMObot
Raul Vargas
PROJECT NAME: miniSUMObot TEAM MEMBERS: Miguel Bin Cantu Bot Raul Hex PROJECT DESCRIPTION SUMObot based in MSP430 LaunchPad PROJECT FEATURES: Simple Code and Electronics Recycled and Cheap Materials UNDER CONSTRUCTION 50% complete Materials: 2 DC gear motors(the gearmotors...
on
Mar 23, 2012
File:
MSP43-oTouch
Aldo Plaku
PROJECT NAME: oTouch TEAM MEMBERS: Aldo Plaku PROJECT DESCRIPTION The oTouch is a touch screen interface for the MSP430 Launchpad. Dip switches and push buttons just aren't cool anymore. With a touchsreen you're no longer tied to digital inputs. Now the input can be...
on
Jul 29, 2011
File:
msPROBOT V1.2
Parker Dillmann
Here is the work log of my msPROBOT robot booster pack for the Ti LaunchPad. It is currently in V1.2 which was the first production PCB. I am currently working on V1.3 which has a better layout, pads for SMD sensors, and a better motor controller.
on
May 25, 2012
1
2