Browse by Tags
Microcontroller Projects
blank
Join group
Get this RSS feed
Tags
430
android
arrays
bluetooth
Booster Pack
clock
controller
Co-op design challenge
game
GSM modem interface with launchpad
LaunchPad
LCD
lcd msp430 display
LED
matrix
MSP
MSP430G2452
msp430g2553
MSPGCC
music
RGB LED
sensors
Servo
TI
Wireless
Related Posts
File:
A Weekly Thermostat with the MSP430
Ruffin White-Magner
PROJECT NAME: My MSP430 LaunchPad Project TEAM MEMBERS: Ruffin White Michael Yuhas Video Link: http://youtu.be/0rrDt5NaOX8 PROJECT DESCRIPTION Normal 0 false false false EN-US X-NONE X-NONE ...
on
Jul 29, 2011
File:
Audio Input / Output Switchbox
Evan Cornell
Audio Input / Output Switchbox TEAM MEMBERS Evan Cornell (corneled@rose-hulman.edu) PROJECT DESCRIPTION This project utilizes the MSP430 to switch between several audio input and output options. The purpose of this project is to be able to choose an audio source...
on
Jul 27, 2011
File:
CardioDroid - Connecting TI and Android
Daniel Ogilvie
CardioDroid Connecting TI and Android TEAM MEMBERS: Daniel Ogilvie, Junior, University of Texas at Austin Michael Sherman, Sophomore, University of Texas at Dallas Blessing Oskaue, Freshman, University of Texas at Dallas Voting is now open! Vote HERE for CardioDroid ...
on
Jul 28, 2011
File:
embedXcode — Use Xcode to develop for LaunchPad platform!
Rei VILO
Use Xcode to develop for LaunchPad platform! embedXcode is a full Xcode 4 template. Thanks to its modular structure, embedXcode can implement virtually all Processing-based IDEs and platforms. It relies on Energia Arduino-based IDE and currently supports the MSP430G2xxx , MSP430FR5739 and Stellaris...
on
Apr 7, 2012
File:
EZ MSP Project
Giovanni Montoya95039
The EZ MSP Project is an ongoing effort to develop easy to use high level libraries for value line microcontrollers. The current release of the EZ MSP Project Libraries contain libraries for HD4780 displays, Timer A generated PWM, and bit banged PWM. These libraries make working with lcd displays and...
on
Mar 5, 2012
File:
GSM interface with Launchpad
RAJESH SHANMUGAM
In This project we are using MSP430 launchpad kit and GSM modem. Based on The Messages PW1/PW2/PW3 the RGB LED will glow in different Color. For demo and Code visit http://embed4u.com/?s=msp430
on
Nov 19, 2012
File:
IV-18 VFD Clock BoosterPack
cubeberg
PROJECT DESCRIPTION IV-18 VFD Clock Boosterpack Click here for documentation and project thread PROJECT FEATURES: Retro look Compatible with the MSP430 Launchpad Time configurable via Serial PCB Design and code open-source **I can't seem to post the youtube videos - so they're...
on
Apr 23, 2013
File:
LaunchPad Learner
Rachel Quinn
See also: n-back Research Video -- University of Michigan researchers discuss their findings on a study of the benefits of n-back. BY: John Hermiz [j-hermiz@ti.com] Rachel Quinn [rachel.quinn@ti.com] Daniel Schucker [d-schucker@ti.com] ...
on
Jul 28, 2011
File:
LightPad (Mobile Light Effects Controller)
Aldo Briano
Project Members: Aldo Briano Stanford University (abriano@stanford.edu) Overview LightPad lights up a room to the creativity of its user and the rhythm of the music. It is an Android hardware accessory that communicates wirelessly to the phone. LightPad's intuitive interface...
on
Jul 27, 2011
File:
Metronome - simple yet awesome, with speed in/decrease and toggling LEDs
Thu Pham
This is a very simple but applicable and useful demonstration for the Texas Instruments Launchpad with a MSP430G2231/11. It shows basic usage of the Port1 as an output and uses interrupts to change the behavior of the program. One simple application is a Metronome that consists only of the MSP430G2231...
on
Oct 21, 2011
File:
Music2Go
Agatha Oliveira
PROJECT NAME Music2Go TEAM MEMBERS Jaime Caicedo Agatha Oliveira Jorge Reynaga PROJECT DESCRIPTION The goal of this project was to provide users with the capability to play music wherever they go. This product uses two microcontrollers MSP430G2452, the capacitive touch...
on
Jul 29, 2011
File:
RGB LED Coffee Table
Mark Labbato
TEAM MEMBERS: Max Thrun Ian Cathey Mark Labbato PROJECT DESCRIPTION This is not your Grandma's coffee table! Make your living room the center of the party. The lights will dance and flash to your music! You will be mesmerized for hours. (We were...) PROJECT FEATURES:...
on
Jul 29, 2011
File:
Scrolling text using several "daisy-chained" 8x8 LED Matrix blocks
AdrianFer
Here's a cool project that leverages the 8x8 LED Matrix BoosterPack from Olimex! This code allows scrolling text/characters across several blocks. This code is written to support 4 8x8 LED blocks to be daisy-chained together, creating a 32x8 LED matrix. (Please visit the site to view this file...
on
Jul 27, 2012
File:
The Terminal - 128*64 OLED Booster Pack
queirarard
PROJECT NAME: The Terminal - 128*64 OLED Booster Pack Developed by: 43oh/Community PROJECT DESCRIPTION The Terminal backpack on top of the Launchpad. An OLED provides high angle viewability and also acts as a crisp display. The driver on this OLED is based on the SSD1306. PCB and drivers...
on
Nov 1, 2011
File:
Using the TI MSP430G2553 to Build a Serial Six Channel RC Servo Controller
Eric Gregori
Using the TI MSP430G2553 to Build a Serial Six Channel RC Servo Controller by Eric Gregori TI MSP430G2553 The MSP430G2553 ( http://www.ti.com/product/MSP430G2553 ) is the biggest part listed in the TI Value Line. 16K of Flash, 512 Bytes of SRAM, 10bit - 8Channel ADC, UART -- In a...
on
Sep 28, 2011