Motor Drive & Control Solutions

Motor Drive & Control Blog

Motor Drive & Control

Motor Drive & Control

TI is a global market leader that leverages its rich history in advanced motor drive and control, with broad analog and microcontroller portfolios, to deliver complete motor system solutions.

  • Understanding thermal properties of motor drivers

    • 0 Comments
    When I think about thermal concerns related to integrated motor driver products, it takes me back to high school physics and a memory that has stuck with me ever since. The teacher was using a hand crank to turn a motor which was acting as a generator...
  • How to have it all: Designing next-generation industrial drive and control systems

    • 0 Comments
    Blog by Sam Sabapathy, C2000™ Microcontroller applications manager, Texas Instruments Developers of next-generation industrial drives systems are always looking for ways to differentiate their drives solution from competition by implementing...
  • Get your motor running: Brushed DC motor driver selection

    • 3 Comments
    In my last blog I discussed how to select a stepper motor driver and in today’s post, I want to continue the series by discussing how t o select a brushed DC motor driver. Integrated brushed DC drivers are much simpler than stepper or brushless...
  • Have you considered using back-emf observers for sensorless speed estimation?

    • 1 Comments
    Sensorless control is gaining in popularity for motor drive applications which don’t demand precise control, below 10% rated speed. A fan or pump drives that operate within 20% to 100% speed range are the right candidates for sensorless control...
  • Tips for driving solenoids

    • 0 Comments
    On the surface, you might think driving a solenoid or valve actuator seams quite simple. And to be honest, in most cases it is. It’s not too terribly difficult to turn current on or off. But, what if your application requires very fast turn on ...
  • Teaching Old Motors New Tricks

    • 5 Comments
    Dave Wilson, Motion Products Evangelist, Texas Instruments One of the favorite parts of my job at TI is going out into the field, meeting with our customers, and conducting motor control seminars. It gives me the opportunity to see what is important...
  • Speed control: the next big thing for sensored BLDC

    • 0 Comments
    Most brushless DC motor controllers operate sort of like the gas pedal of a car. If the pedal is pushed down some amount, the car will travel at different speeds depending on if it’s climbing a hill, going downhill, or plowing through snow. ...
  • Simulation Power!

    • 2 Comments
    Dave Wilson, Motion Products Evangelist, Texas Instruments As many of you know, I am a BIG fan of using simulation tools to unlock the mysteries of the motor control universe. With embedded model-to-code options from VisSim, PSIM, PLECS and Simulink...
  • Spin It! - Designing Your Own Motor Drive and Control System (Part 4)

    • 0 Comments
    Part 4: Dos and don’ts of layout design Howdy and welcome back! In my previous posts , we pieced together a system, found our components, conquered the mighty schematic, and reviewed, reviewed, and reviewed some more. Many people will call...
  • Why the future of motor drive and control is so important (Part 2)

    • 0 Comments
    Tim Adcock is the director of the TI Kilby Labs Motor Lab. In Part 1 of Tim’s post, he outlined the future of motor drive and control on the TI official company blog. In Part 2, Tim explains the motor drive and control technology TI has developed...
  • How to use a speed table for easy nonlinear input-to-output response

    • 0 Comments
    In motor applications, it’s suitable to respond to a varying input command with a nonlinear output response to allow compensation for a machine limitation and to provide a better user experience. For example, in an application with an analog input...
  • Generate your own commutation table – part 2

    • 4 Comments
    In the previous blog, we discussed that deriving the right commutation table plays an important role in controlling 3-phase BLDC motors using hall sensors . As a refresher, here are some surprising facts about the drive system: Out of six possible...
  • The art of stopping a motor – VM pumping

    • 1 Comments
    In my last post we talked about methods to stop a motor . As a refresher, check out the table below. In this post, we will dive deeper into the VM pumping mechanism and how to avoid the pumping. When and how is VM pumping up? In one...
  • Spin It! - Designing Your Own Motor Drive and Control System (Part 3)

    • 0 Comments
    Part 3: Schematic Capture Howdy! Welcome back or if this is your first time here you can check out the rest of the series at Spin It! - Part 1 (Introduction) and Spin It! - Part 2 (Component Selection) . We have our idea in mind, we have our...
  • 15 tools of the trade

    • 7 Comments
    We use quite an assortment of equipment in our motor labs. The right tools for the job make all the difference! Let’s dig in. 1. Laser tachometer This device shines a laser and measures the frequency of reflective pulses. The rotor being...
  • More than just motors: low-side drivers

    • 0 Comments
    Motors are the coolest! They’re one of the basic elements that make the modern life possible: they knit our clothes (textile machinery), provide us with snacks and drinks (vending machine), keep our rooms cool when it’s 100 degrees outside...
  • TI unveils InstaSPIN™-MOTION with position control!

    • 2 Comments
    Motor designers can now build embedded position servo systems quickly thanks to a suite of motion and control products in InstaSPIN-MOTION . Adding to the revolutionary InstaSPIN motor control technology, InstaSPIN-MOTION expands upon its offering of...
  • TI showcases an in-depth look at never-before-seen technology for motor control, drives and PLC applications at SPS IPC Drives in Germany

    • 4 Comments
    Taking the opportunity to unveil three new embedded processors coming to the market in the next year, TI will demonstrate these products in action at the largest industrial show in the world. The target applications include: High-end drives,...
  • Generate your own commutation table: Trapezoidal control 3-phase BLDC motors using hall sensors

    • 2 Comments
    A couple decades back, if you asked motor control engineers which type of motor they prefer the answer without hesitation would have been a brushed DC motor . That’s because brushed DC motors are the simplest to control. You just apply DC voltage...
  • You will not be able to spin this motor

    • 5 Comments
    THE CHALLENGE I was on a business trip earlier this week to visit some customers, and as always I arrived looking to spin motors. The first visit was well planned; one of the engineers had previously attended an InstaSPIN workshop and wanted me...
  • Motor development in the palm of your hand! BOOSTXL-DRV8301 BoosterPack!

    • 7 Comments
    I’m sure many of you are familiar with the LaunchPad/BoosterPack Ecosystem developed at Texas Instruments. Well, we in the Motor Drive business decided to make our own contribution in the form of the BOOSTXL-DRV8301 ! It is common practice to pair...
  • Get Your Motor Running: Simplifying the stepper driver selection

    • 1 Comments
    Changing one’s perspective can be a very enlightening exercise. I just recently purchased a new car and found myself on the other end of the transaction – I was the buyer, not the seller. You would think selecting a car would be easier than...
  • Increase Your Motor Iq

    • 1 Comments
    Dave Wilson, Motion Products Evangelist, Texas Instruments As engineers, we often have to choose between activities that enrich our careers versus those that enrich our employer’s bottom line. That’s why it’s so refreshing to find...
  • Easy cruise control for brushed motors using BEMF

    • 6 Comments
    Brushed motors are the most common and lowest cost motor type in use today - nearly 10 billion brushed motors ship every year. Even though these motors are simple, it is very easy to add somewhat advanced features such as closed loop speed control , or...
  • The art of stopping a motor

    • 0 Comments
    When starting to develop a motor driver system, most of the attention is focused on initially spinning the motor. But soon after the successful spin, you may find that it is also very important and even more challenging to stop the motor properly. You...