Hi Eric,
We have some great selection of voltage references in the link below. For instance, REF35 , REF50xx , REF60xx , REF70 and many other low cost, low noise, very low drift precision voltage reference for the ADC application.
https://www.ti.com/power-management…
Hey Vijay,
If the power supply is +/-15V and the output were to get pulled to either +/- 5V than the output isn't reaching a potential beyond the supply and therefore within the specified operating range of the device. If the output goes positive on a…
Hi Cyrille,
Cyrille Najean said: it will be mandatory to perform those tests on every component batch that will be use.
From the high temperature instrumentation amplifier (IA) selection, we have the following possibilities that the operating temperature…
Hi Abi,
Abigail Leonardi said: Given the 0-2.5V input signal and a 0-5V output, there is only need for a gain of two from the amplifier.
Enclosed are alternative power amplifiers that may meet the requirements, see the link below.
https://www.ti.com…
Hi Chirag,
Chirag Panchal2 said: I would be grateful if you could suggest an instrumentation amplifier/s (I would like to keep unity gain).
You are correct. I do not see anything special about LT6012CS opamp. It is costly to build an instrumentation amplifier…
Hi Sk,
If you are looking for 1.5MHz to 1.5GHz Op Amp, the product is supported by High Speed Amplifier, see the search link below.
The precision op amp support team covers the Op Amp with BW up to 50MHz. Please take a look at the link below, and I will…
Hey Zhaowen,
So the pk-pk noise with 35kHz input and output filters is still 30mV? This is too high. I calculate something closer to 3mV pk-pk. To make sure you are measuring the true operational noise for any amplifier make sure you do the following…