F280013x and F28002x series are TI Quality Managed.
They can be used in IEC60730/UL type of appliance applications as well as checker micros in SIL systems.
Part Number: MSPM0C1104 Hello,
my colleague and I are currently developing two new appliances using MSPM0C1104 MCU and now found out, that in the datasheet position of SWDIO and SWCLK is sometimes mixed up and we do not know which version is correct one…
Dear Jeff, Thank you.
BQ24650 and BQ24210 sound good! Do they also support charging a super capacitor after the Li battery in the question has been fully charged?
Could you provide their officially tested reference designs?
Actually, I have a fully working…
Hi Kazuya,
Thanks for reaching out!
Please refer the comments below:
1. LP5860(T) family is a matrix topology LED driver. Please refer the simplified schematic below, it has 18ch constant current sink and also has 11 line switch to build the matrix topology…
Adam,
Yes - There is no need to increase switching frequency for faster response, that is because C2000 MCU's ePWM peripheral can update duty value in the same cycle with "Direct Load Mode". It means that it will change the duty within the same cycle. But…
Part Number: ULC1001 Other Parts Discussed in Thread: ULC-HPB-DEMO hello,
Could you please tell me the model number of the AC adapter included with ULC-HPB-DEMO or the recommended specifications?
Our customers must purchase an AC adapter that is compliant…
Hi James,
TPS25751 is meant for power-only applications such as battery chargers, personal electronics such as bluetooth speakers, and other appliances that does not require additional alternate modes such as DisplayPort, Thunderbolt, USB4, etc.
What…
I have a customer that he have developed a motor system,the motor system is made for small appliances.The motor system is a discrete scheme.
Does TI have a better scheme to replace the discrete scheme
input voltage :36V
Hi Arvind,
"Should this external circuit will help for mitigating this problem ??" - I do not know, it may help - it may not.
You are experiencing driver IC failure that can be caused by design errors as well by external factors.
One serious…
Hello GR,
The BQ202x is built on EPROM memory, which is a one time programmable memory (OTP). In other words, once the intial bit is changed from a 1 to a 0 the bit can not be changed back. This works great for applications that need a small memory device…