Part Number: LMX2820 Currently I'm struggling to change the frequency on the LMX2820 via a FPGA. I'm able to do the default setup on the PLL and get it too lock and output the default frequency of 13.05 GHz. But when only changing the frequencies by updating…
Part Number: DAC38RF82EVM Hi,
I am looking for a sample FPGA project using DAC38RF82EVM + iwave iW-RainboW-G30D (Zynq Ultrascale+ MPSoC (ZU4) SOM)
Thanks, Divya.
Part Number: ADS5296A Hello Iam looking for an EVB with the following requirements
- 4 a2d channels
- sampling rate >= 20 MSPS
- interface serial lvds to fpga (no jesd)
- resolution : around 10 bits
need help to find such a board ..
if the evaluatoin…
Part Number: TMDSEVM6678 XILINX_XC3S200AN is being used in the evaluation module, and we need the internal code of this FPGA. Where can I download it? Setting values for CDCE62005RGZT and UCD9222RGZR are required.
Part Number: ADC12DJ5200RF hello,
I have a LVDS output from a Xilinx Ultrascale+FPGA and would like to connect it to the TMSTP inputs.
Unfortunately the DC-coupled TMSTP must meet the low common mode voltage requirements, which is not compatible with…
Sorry Simon, but nothing from our side. We are just not familiar with power solutions. It is interesting that you can't post a general power question on that forum. They may have folks assigned to different products but somehow someone should be looking…
Part Number: TPSM63610 Hi there,
I am using TPSM63610 in my project for three applications (28V to 12V, 28V to 8.5V and 12V to 4V conversion). In the datasheet (reference schematic in the datasheet) as well in TI WEBENCH circuit designer, the IC is being…
Hi Juliette,
Just wanted to check if there was any update on this. I'm still trying to find the best way of supplying the clean 5V for the DDC232 with whatever power chips are available from TI.
Simon.
Part Number: SN75LVCP601EVM Other Parts Discussed in Thread: SN75LVCP601 , We have in-house developed SATA Host IP ported on standard off-the shelf Xilinx FPGA platform. we use GTY transceiver configured for SATA PHY applications. currently we see link…
Part Number: TSW14DL3200EVM Other Parts Discussed in Thread: ADC12DL2500EVM I'm looking to reprogram the onboard FPGA so that I can use the external trigger TRIG_IN SMA connector as well as access the raw data coming from the ADC12DL2500EVM. According…