Part Number: DAC53701 I use an stm32g031 mcu and two dac53701.
i found i have already changed one of the two dacs's slave address,but when i set to generate wave,,the two dac outputs are 0V.
schematic and code is below
void SetGpiVal(uint8_t dat…
Amazing! This should be enough to get me going :))
Thank you so much for your insight and expertise Shabbir. This is very much appreciated.
I wish you all the best.
Benjamin
Part Number: CC3220R Hello everyone,
I will be designing a small datalogger with very basic functionalities and WiFi and Bluetooth connectivity for a hospital. The only external hardware I will use is an ADS1148IRHBR for sensor measurements, an LCD screen…
Part Number: IWR6843
Hi,
Good Day.
I'm doing some research on the IWR6843. Do you know if it is possible to get an approval this sensor as a medical device? And if not, do you have a similar product that does? I should add, that I want to distribute…
Part Number: LMR50410-Q1 Hi,
We have a design, built in 2021 and as its a medical product we had to go through all the testing and approvals and it took us some time to complete them. Now we want to build few of these products but we are short of LMR50410YQDBVRQ1…
Part Number: DRV8428 Dear Teams,
I would like to use this product for an FDA Class II medical equipment. It is not a life-critical medical equipment. Do I need a special permit to use the parts? Please let me know if there are any restrictions such as the…
Part Number: TRS3122E Dear Teams,
I would like to use this product for an FDA Class II medical equipment. It is not a life-critical medical equipment. Do I need a special permit to use the parts? Please let me know if there are any restrictions such as…