Part Number: TPS3110 Hello,
In the TPS3110E15DBV, we noticed that the time out period is 1.1 seconds, do we have any alternatives that have a time out delay of 2 seconds?
Part Number: TPS3808
Supervisor selection for DSP TMS320F28377:
The VDDIO and VDD of DSP are powered by 5V/3.3V LDO1( ADP3339AKCZ-3.3) and 3.3V/1.2V LDO2(AMS1117-1.2) respectively.
The minimum output of LDO1 is Vcc1_min= 3.2373V (-1.9% of 3.3V).
The minimum…
Hi Tim,
Any of the TPS65219 variants can be supplied by 3.3V or 5V (as long as the PMIC outputs are configured for <3.3V). This means TPS65219 02 can be used for 5V Vin, LPDDR4, CORE=0.75V or 3.3V Vin, LPDDR4, CORE=0.75V . For the 5V Vin, the external…
Hello,
I require a voltage supervisor that detects overvoltage of VTI only. Due to stock levels and project requirements I've found the TPS37043BJOFDDFRQ1 suitable for our application.
The datasheet says it can be configured to either OV, UV or both…
Part Number: LP3470A Hi team,
My customer is checking spec of LP3470A to utilize this on their project.
This has SRT(Set Reset Timeout) pin to make reset delay time by connecting external capacitor. (other similar device, it specified CT(Capacitor Time…
Hi,
do we have p2p alternatives to these ADI parts.
TI BOM tool did not find anything.
AD45325 Ultra-Low-Noise, High-Accuracy 2.5V Voltage Reference DS1832S+ Supervisory Circuits Supervisory Circuits 3.3 Volt MicroMonitor Chip
Thanks
Josef
Part Number: MSP430FR4132 As per section 2.2.2.1 of user manual we have SVS thresholds namely SVS H_IT+ and SVS H_IT- . Based on these thresholds we get Brownout reset. But in user manual
Part Number: TPS3704-Q1 Hi expert,
My customer is choosing a supervisor for F28377D.
They found TPS37042 is good for them. But they still have two questions:
Question1. we have many choice listed on datasheet, this is what they want to choose:
but I…