Part Number: PROCESSOR-SDK-DRA8X-TDA4X
My OpenVX application is hanging when pipelining with an OpenVX object array when calling vxGraphParameterDequeueDoneRef. The producer node is a replicated node that is outputting an element of an object array. There…
Part Number: PROCESSOR-SDK-DRA8X-TDA4X
I am trying to create a pipelined graph in OpenVX. My application is a 2 camera capture application where I want to process these channels in separate downstream nodes. I see that the output of the capture node is…
Part Number: PROCESSOR-SDK-DRA8X-TDA4X I see there is only one target option for assigning a given OpenVX node to one of J7’s heterogeneous cores. If I have multiple nodes that need to run on one of these cores, how is this treated by the framework? Do…
Part Number: PROCESSOR-SDK-DRA8X-TDA4X I have two algorithms that I would like to use on a given core within J7. Should I wrap these algorithms into two different OpenVX nodes within my OpenVX graph or should they be a single node?
Part Number: PROCESSOR-SDK-DRA8X-TDA4X
I get the following error messages during vxVerifyGraph in OpenVX. How do I fix this issue?
VX_ZONE_ERROR:[ownContextSendCmd:553] Command ack message returned failure cmd_status: -1
VX_ZONE_ERROR:[ownNodeKernelInit…
Part Number: PROCESSOR-SDK-DRA8X-TDA4X
When I try to create a new node in OpenVX, I get the following error message on the target CPU:
"tivxTargetKernelInstanceAlloc: kernel <kernel name> has not been registered on this CPU"
I also get…
Part Number: PROCESSOR-SDK-DRA8X-TDA4X
When I try to create a new node in OpenVX, I get the following error message. How do I fix this issue?
"tivxCreateNodeByKernelName: Call to vxGetKernelByName failed; kernel may not be registered"
Part Number: PROCESSOR-SDK-DRA8X-TDA4X
Dear Users,
The Jacinto 7 FAQs are now made available.
To navigate FAQs for a specific module, please follow the link below:
All
Boot
C7x
DMSC
Graphics
Imaging
MCAL
Networking
OpenVX
QNX
Safety
We hope that you…
Part Number: PROCESSOR-SDK-DRA8X-TDA4X
I see that TI supports OpenVX, but I don't see an openvx folder in the SDK, only a tiovx. Is this the same as OpenVX or are there differences?
Part Number: PROCESSOR-SDK-DRA8X-TDA4X
I would like to use TI's OpenVX for application development. What are the kernels that are supported by TI's OpenVX that can be used in my application?