• TI Thinks Resolved

TPA61111A2 SHUTDOWN PIN

Only mention of the Shutdown pin in the data is "Puts the device in a low quiescent current mode when held high". If I don't need this function, which I don't believe I do, can the pin just be tied to ground? Is this pin needed to reduce the "start up pop" or not required if the R/C value rules are following in the application information.