This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DRV602 and DRV603 Turn-on/off Times

Turn-on and turn-off times for DRV602 and DRV603 are nominally 1mS and 300uS.  They vary with the charge pump oscillator frequency, +/-50%.  They are independent of decoupling and charge pump capacitor values unless these are made significantly larger than recommended values.  Users wishing to use values larger than the recommended values are encouraged to verify the effect on turn-on/off times if that is important to them.

  • Steve,

    You sure do like those DRV60x parts, don't you? they are some mighty fine audio line drivers!

    -d2

    Best regards,

    Don Dapkus

    Gate Driver Applications Engineering Manager

    Dallas, TX USA

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.