Application:
1000W sonar driver.
Vout 500V or greater
Drive underwater transducer for sea floor distance measurement.
15khz +-3khz modulated output, modulated for sonar signal Identification.
20ms pulse every 5 seconds, max every 1 second for testing, very low duty cycle. Low average power.
I am considering a full bridge with the AC signal used as the error amp reference.
Turns ratio to get the voltage up to drive the transducer.
Do we have any examples of TI Audio devices being used for SONAR?
Transformers would be needed to increase the output voltage.