Hi Don, I hope your well. Im interested in the 5631EVM. It appears to come with '5518 which is an EOL part. Is there a new EVM with an audio processor that is not EOL? Also it appears that the USB input board will accept 192K in via S/PDIF andthe AKM4113. Will the full EVM support all rates from 44-192? I'd like to be able to feed the system 44/48/96/192 without any mucking with the jumpers or software. Will it support this?
Cheers...Doug
Hi, Doug,
Sorry I missed your post.
Did you get this sorted out?
-d2
PS TAS5518 is NOT EOL, it's NRND. Big, big, BIG difference. We have no plans to discontinue production of the TAS5518. Also, TAS5508C, which is pin-compatible with it, is still being actively promoted for new designs. And, we've got some new modulator ICs in the pipe coming out later this year... Not pin to pin. I obviously can't discuss proprietary info on e2e, you should contact your local sales office for more information on products in development.
-----
Don Dapkus
Audio Applications Engineering Manager
Dallas, TX USA