Hi,
I would like to know if it is possible to set TAS5602 as follow:
1 SE output = 2.5W
1 BTL output = 35W
Thanks.
Joe
Hi, Joe,
It seems like that will work if you use 24V and 8 ohm loads. However, it might not thermally work as too much heat will be centered on the BTL channel. You may need to add some external heat sinking.
What are you planning to use to generate the PWM input signal to the TAS5602?
-d2
-----
Don Dapkus
Audio Applications Engineering Manager
Dallas, TX USA