Hi Folks,
I'm hoping these are a simple questions; I've just started working with the TPA2028D1 and there are a few things the datasheet isn't clear on:
1. How do you disable the AGC? This is mentioned prominently in the datasheet, but I can't find an explanation of how this is done.
2. How do you set the volume output? It seems to be done using the "Fixed Gain", but I don't seem to be able to get the kind of changes in volume that I would expect.
3. Is there a way to "mute" the output? I would like to turn off the amplifier - is the "EN" bit of the IC Function Control register the right way to do this?
I do have a couple of the the TPA2028D1YZEVM's, and have wired them into prototype circuits (I can peek and poke the I2C registers and verify that I'm making changes) but I can't get the software to work - looking in the forums, there seems to be a "5100.drivers.zip" download, but I can't access that.
Thanx for your help!
myke