Hello,
we have plenty of experience with TAS 5518 and TAS 5508 together with TAS5342. Now we are going to change our design to the new TAS 5548. We designed new circuit boards manly based on our old design for SE, Bridged and Parallel Mode of the TAS5342.
Unfortunately, in out test design, after some time of working correctly, we cannot write to the Status Register 1 and 2 (0x03 and 0x04) any more. All other registers seem to work ok. Unfortuneately 0x03 is necessary to end shutdown mode and 0x04 to stop Auto-power-off. Therefore, everything don't work any more.
Ending shutdown mode seems to be the crucial point. Bit D4 cannot be altered. but D7 or D6 work. Playing around with individual channel shutdowns in register 0x27 can make it possible to be able to alter D4 in 0x3 but this does not seem to work all the time. Nevertheless, since the occurence of the described problem, we did not manage to make the design work anymore. Reset and power off do not help.
What is happening? We are completely at a loss. Maybe there are errors in out design - although it worked with TAS5508 without problems. Or are there some properties of the TAS5548 we did not notice?
Thank you for yout help.
Cornelius Bradter