On the TPA3116 FAULTZ can be linked to SDZ to shutdown on a fault. However, since these 2 pins are linked, is it still save to MUTE the amplifier as it is also connected to FAULTZ ?
It does not seem to say either way in the datasheet, it does list driving MUTE, but it is not connected to FAULTZ. My concern is, as FAULTZ is a output, will it blow the chip if this is also connected to MUTE which can be controlled my a MCU etc ?