Figure 5 in application note AN-1651 ("Keeping up with the Expanding Demands of High-Performance Audio") would seem replete with errors and should be corrected. Balance Potentiometer R11 referenced in the text is missing from the schematic, perhaps one should assume that it is between the sources of the output transistors with the wiper connected to the input of the LM317. Should the drain of Q1 should be connected to the output node via C6? The negative power supply is labeled incorrectly.