Hi
I’ve been evaluating the TAS5731M class D amp for possible use in a new product and don’t seem to be able to achieve the specified power o/p into 4/8 ohms.
Please see outline of issues I’m encountering below:
I am currently evaluating the TAS5731M (higher power version of the TAS5731) using the TAS5731 dev board.
In 2.0 BTL mode when checking the maximum power at 1k into various loads I found that I could only achieve 30Wx2 into 8R 10% THD (60W tot) with max PSU voltage of 21V and 20Wx2 into 4R approx 0.4% THD (40W tot) with a max PSU voltage of 20V. Beyond these powers the device shut down immediately. Note that these were pretty much instantaneous tests only switching on for less than 10 seconds to minimize heating effect.
The graph on p18 of the data sheet shows that should be able to achieve 35W into 8R (x2?) with 24V PSU and 40W into 4R (x2?)with 20V PSU in BTL 2.0 mode with the 2 layer Evaluation PCB.
I think that over current/over temp flag is being set by the amplifier but cannot check to confirm because over current /over temp flag in the error status x02 register is not shown in the I2C output in the graphical GUI (is there a way to show this?). Also thinking the heat sinking has to be completely optimal to achieve high O/P powers.
Also note the following additional comments on setup/configuration:
All filters set to flat freq response. DRC off.
Have fitted large aluminium block completely flush to bottom of eval board with heat sink compound for max heat dissipation.
Please can you assist with understanding this issue.
Also would like confirmation that the o/p power graph for 2.0 BTL mode (p18)is for both channels driven as this is not explicitly mentioned.
Finally could it be possible that the default over current setting trip for the original TAS5731 is still set for the TAS5731M somehow?
The TAS5731M is attractive since it has the integrated DSP and also allows us to independently EQ channels individually ( ie not ganged) for the speaker product that we’re developing.