Hello. I need to use a class-D amp to drive a
DC inductive load.. (big solenoid used for positioning)
I was going to use the TPA3106 - it appears to have DC
continuity throughout the device, and a differential input.
(seems perfect) Has anyone done this, and
if the answer is "no, don't use it for that" can they recommend
a class-D that is good for DC applications?