Hi Sir
An specification, “Maximum Input Voltage = 2Vrms (Typ) @ EN = 0 ” listed in electrical characteristics.
Since EN = 0, device is inactive, and 2Vrms = 2.828Vpeak that is not beyond the absolute input maximum rating = VBAT + 0.3V (6+ 0.3 = 6.3V)
(1) What is the specification intended for?
(2) If stimulus = 2Vrms @ EN = 1, other than output saturation, is there any risk in application or damage?
As other product of audio amplifier such as TPA2010D1 has no clear definition to maximum input voltage, but found inside TPA2080D1, there must be a reason!
Greatly appreciate for your answer
Thanks
Regards
Ben