I have purchased a TPA3118 board similar to this one:
www.ebay.com/itm/TPA3118D2-Digital-Audio-Power-Amplifier-Assembled-Board-Dual-Track-25W-25W-Mono-/171356434400?pt=US_Amplifier_Parts_Components&hash=item27e5a3afe0
I put 8 ohm 40 watt resistors on both output channels. I then injected a 1 kHz tone into the left channel and ran the amplifier up to the 18 watts power level. I let the board run for 30 minutes and measured the temperature of the TPA3118. It measured 55 degrees C.
Is this a safe temperature for the device? The datasheet shows a maximum of 150 degrees C. The real world application will be for music so the average power level will be nowhere near the level I was running in my test. However, if I had driven both channels, the part may have gotten much hotter.
Also, would anything be gained by expoxying a small heat sink to the top of the device or is the die to case heat transfer too low to help?
Thank you.