Hi,
My customer has a problem with TAS5715EVM. Althogh the customer has tried to make the EVM work, he cannot make it yet. Could you give me something advice?
The situation is as below.
- Latest GUI is downloaded from TI Web site : Ver3.2, build7
- I2C address setting : 54 --- Refered "SLAA484 : Setting TAS5715EVM Environment Variables"
- Select "TAS5715" device
- After "Power On" and "Target connect", "Shut down" and "Mute" is set "OFF"
Then "small pop noise" has happened but no music is reproduced...
- But in case of device selection is "TAS5717" not TAS5715, music is reproduced but volume control is uncontrollable...
It's very strange.
- The customer's PCs environment is as follows. (The customer has tried on 3 PCs.)
Windows7 Professional Service Pack1 32bit, Windows8 32Bit
Intel® Core™ i5-2520M CPU @ 2.50GHz, 2GB/4GB RAM
The same situation(behavior) on both Win7 and Win8.
- I also tried to make the EVM work on my PC and I could succeed to make it.
My PC's environment is almost same as the customer's one. Only customer's PCs cannot make it.
It's very very strange.
Now we are in problem and cannot find the solution.
Could you please give us any advice about this?
Best Regards,