How does it work. The spec sheet says when it stabilizes then outputs are connected. Would this not cause a pop?
I am referencing this from sheet 19 of datasheet.
The gain of the internal amplifiers remains unity until the voltage on the bypass pin reaches VDD/2. As soon as
the voltage on the bypass pin is stable, the device becomes fully operational and the amplifier outputs are
reconnected to their respective output pins. Although the BYPASS pin current cannot be modified, changing the
size of CBYPASS alters the device's turn-on time.