Hi,
We have evaluated the frequency response to verify the low cut-off frequency with HybridFlow1 using TAS5754M evm.
As a result, it is about 30Hz, this frequency is the -3dB point for the gain of 1kHz.
Biquad and DRC are the all path mode, DBE, PBE and other is default settings, the output load is the pure resistance of 6ohm.
Then, is it possible to decrease the low cut-off frequency to 10Hz?
Could you please tell us that procedure if it is possible?
Best Regards,
Kato