Hi,
We are using TPA2051D3 amplifier. Please suggest for the following questions.
1) The datasheet says VIH(min)= 1.3V and VIL(max)=0.3V for VDD=1.8V and VIH(min)= 3V VIL(max)=0.3V for VDD=3.3V. Can you suggest what will be VIH and VIL values for VDD=2.9V.
2) Datasheet says the maximum delay time between AVDD and PVDD to DVDD (tpws) is 100us. We have a test case when AVDD and PVDD will be ON but DVDD will be off So what happens in this case and what happens when DVDD is applied after that. You have a suggested a resistor divider if tpws is more than 100us but in our case AVDD is a variable voltage so we cant keep DVDD constant if we use resistor divider.
3) Can we give differential input to the stereo input lines (INL1,INL2, INR1, INR2).
Regards,
Sateesh