Hi,
Please suggest for the below queries related to TPA2051D3.
1) According to TPA2051D3 datasheet the delay tpws should be less than 100us.
In our case AVDD is connected to Battery voltage. Consider following cases
case (i) if AVDD is > 3.3V, DVDD will be always present and within time tpws .
case ii) If AVDD is < 3.3V, DVDD will be off but AVDD will be on (<3.3V) so the only way that DVDD can get on is through charging and once the charger is connected we will get DVDD within tpws so the question is whether digital part will work as the delay was lesser than tpws or it doesn't work since AVDD is always on.
2) We can use different voltage for I2C and DVDD according to datasheet.
Lets say I am using DVDD = 2V for TPA2051D3 and the SCL, SDA lines are pulled to 3.3V
which is a valid case as Vih for 3.3 is 3V and DVDD is less than 3V for PVDD = 3.7V.
So on what voltage level does enable work ? Is it 3.3V like the SDA/SCL lines or we should consider DVDD as 2V for Enable.
3) Datasheet says Recommended voltage for DVDD is 1.7 to 3.3. Can the digital part be
still on for 1.2V as it doesn't cross absolute minimum volatge. Does that twps timing rule holds good when DVDD is 1.2V or the DIgital part will be off below 1.7V.
Regards,
Sateesh