Hello,
We have a few Class D ICs running on an audio board with an 18V supply rail being used to drive 8ohm speakers on a bus. Occasionally, the techs out in the field who install the devices might wire the speakers incorrectly and cause a short in the output or supply pins.
According to the datasheet, the ICs should be protected because the output transistors enter a high impedance state. Even if that fails, the device should be protected from thermal runaway by thermal protection.
We have found that the ICs are still blowing up despite the error being improper wiring of the outputs. Any reason as to why this would happen? What other wiring mistakes could cause this problem on the TPA3112D1s?
Should we be adding additional circuit protections?
We're using LTC3891EFE#PBF power supplies. It is unlikely that the slew rate on these is greater than 10V/ms so we haven't placed a 100k resistor in series with the gain pins.
Please let me know.
Thanks,
Pranit