This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5717 query

Other Parts Discussed in Thread: TAS5717

Hello Folks,

We are planning to use TAS5717 in our design. I have a few doubts regarding this power amplifier. I am driving 4 ohms 2 W speaker using this PA. Will it work in that if I provide 5V to PVDD supply?

Looking forward to your quick response

Srijan

  • Hello Srijan,

    TAS5717 supports a PVDD voltage of 5V. I have verified this in the EVM and effectively it is able to drive ~2W in a 4Ω Load with a volume of 0dB gain and an input of 1FFS. 

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer