Hello,
I have already tried to find answers to my questions in the datasheet of the amplifier as well as in the "HybridFlow Processor" manual (SLA577), but I still have some left and so I hope that you can help me with the following things.
1.) How is the program loaded into the HybridFlow Processor?
Is it necessary to buy the "PurePath Console Motherboard (PPCMB)" to configure the DSP? If yes, how am I supposed to connect the motherboard to my own amplifier board (not the EVM)? Do I need to include the same connector that can be found on the EVM on my PCB or is there a different (simpler) way?
2.) Can certain "HybridFlow" settings be changed during operation?
In other words, can parameters like bass, treble and maybe balance be changed via I²C without reprogramming the DSP (and without using the GUI)?
If the amplifier on its own is not capable of this, how could I add this functionality to my project (maybe with an additional IC between the DAC-out and the input of the actual amplifier stage)?
3.) Is it possible to amplify/mix a stereo signal in PBTL-Mode?
I want to drive a single speaker in mono-mode (PBTL), with a stereo signal at the input of the amplifier. Can this be done using the internal DSP or will I have to use external circuitry?
I really appreciate any help you can provide.
Greetings from Austria
Reinhard F.