Hello. I have many TAS5630KDR that fail.
I have more than 10% failure in my design with the TAS5630KDR. The SD Pin goes high and I have short form the output pin "OUT_A" and "OUT_C" to ground.
I was suspecting some over Voltage spikes in the output and made some measurements of the outputs. In the ZIP file below you'll find the design and information to my measurements.
The overvoltage spikes of +/- 15V you'll find in the DSO printouts occur only in the first one or 2 seconds of pin "REST" going high or pin "RESET" going low with audio signal applied to the inputs A + B. with out audio signal the voltage spikes are not occurring. The spikes are independent of the load (3 or 6 Ohm or no load).
I notices also that the spikes occur when the "OUT_A" is still high and the "OUT_D" rises high. I don't understand why "OUT_D" rises while "OUT_A" is still high. I believe these two outputs should not be high at the same time.
The voltage over all "PVDD" pins was during the measurements "clean". There was no voltage overshoots.
I made the measurements with 48VDC. In actual the Voltage can rise up to 54.6VDC. this is the charging voltage for the PB batteries.
I hope this problem can be solved soon. Because there are about 150 amps out in the field and so many are coming back defective.
Greets Dani