We currently use this device in a production product , and now have a new product in design stage. We have noticed that there is an updated datasheet. On the latest revision of the datasheet:
1) There is a reference to single supply operation, but no reference design or additional information to methods for single supply operation. Can anyone please provide additional information on single supply operation of the TPA6120A2.
2) In the datasheet there is an output resistor specified in the reference design which was 10 ohm in the previous datasheet revision and is now 39 ohm - please elaborate as to the reason for that change. Do I need to be concerned about our production product which has 10 ohm output resistors?