Dear all,
I'm using a TAS5558 in combination with two TAS5624 amplifier ICs (6 channels, single ended configuration as described in the TAS5624A datasheet, p. 21). So far everything is fine, there's no pop or click noise when switching on the amplifier. But when I switch it off, there's a strange noise. It sounds like a discharging cap (swoosh noise). There's no better way to describe it.
My power off sequence is:
1. Mute TAS5558 (Softmute all channels)
2. Pull down the reset signal of both TAS5624A amps -> this is when the swoosh noise occurs
3. Switch off TAS5558 (Channel shutdown in register 0x03 -> reset)
4. power off the unit
I've played around a little bit with several register settings in the TAS5558 and I get the best results when I skip the first step (soft muting the TAS5558). The swoosh noise is almost gone but then there's a quiet pop noise. So not an ideal solution.
Now to my questions:
1. Is there any recommended configuration for this setup (TAS5558+TAS5624 SE mode), e.g. register settings, power on/off sequence, etc.?
2. I've also tried the different PWM config setting (legacy lowZ, special lowZ, MidZ) but there's no difference at all. Can you recommend a setting?
Thanks for your help in advance,
Daniel