Hi, I'm getting ready to head into production with the below amplifier and circuit. It's on a 3.3V logic system and I really like the sound of the 4ohm speaker we have chosen. 8ohms is OK, but I know it's a bit out of spec. I would like to know if anyone could elaborate to tell me how likely it would be to fail if possible, or how far out of spec I really am? I suspect I am not driving the amplifier that hard, and it does have a good ground plane heat sink with many vias under the pad. It does not feel warm to touch, and usually used for sound effects, not really continual music. I measure around 2.5-3.0 watt draw roughly when playback.