This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Differences between TAS5XX 、 TAS5548(Pure Path Console)、TAS5508

Other Parts Discussed in Thread: TAS5548, TAS5508, TAS5558, TAS5624A

Dear Sirs,

My Customer asked to  me about differences between TAS5XX and  TAS5548(Pure Path Console).

When the following conditions start the GUI not in check in each set after I2C Logging settings DRC_1 the data had different as follows.
Please tell us about this difference.

      GUI                               EVM              ADRESS      RESISTER       THRESHOLD               DATA

TAS5508                               -                     0x99           DRC_T1               -100dB                   08 4E 08 B2

TAS55xx_GUI     TAS5624AEVM           0X99           DRC_T1               -100dB                   0A 55 55 55

PPC                      TAS5548EVM              0x99           DRC_T1               -100dB                    08 4E 08 B1

 

TAS5508                               -                     0x99           DRC_T1               -58.66dB                04 DF 21 AC

TAS55xx_GUI     TAS5624AEVM           0X99           DRC_T1              -58.66dB                 06 E3 69 D0

PPC                      TAS5548EVM              0x99           DRC_T1               -100dB                    04 DF 21 AB

Also, please tell me TAS5548 of GUI (PPC) can be used in EVM of TAS5624A. (The latest of Userguide is equipped with TAS5558)

TAS5624AEVM of GUI (TAS55XX), please tell me if you can use in EVM of TAS5548. (USB communication was OK)

Best Regards、

Y.HASEBE