Hi,
I have to replace the ST's TDA2030 in an automotive application for obsolescence of the component.
I've successful tested the pin-to-pin compatible TI's LM1874, but I need to know the really operative temperature range:
on product's page description is specified "0 - 70°C"
datasheet's maximum ratings say "-65 - +150°C" of storage temp and "150°C" of junction temp
Than:
- if the limit is on the junction, can I consider to work at 85°C with a proper termal dissipation?
- if my previous hypotesis is true and than the "0 - 70" description is not true, what is the minimun operating temp?
Thank