Customer resister step is below.
(Default setting)
Step w/r reg add data
1 w 00 00 ⇒Page 0
2 w 02 10 ⇒Standby Mode
3 w 03 11 LR Mute:On
4 w xx xx (Writing coef A, B, Instrunction memory)
5 w 00 00 ⇒Page 0
6 w 2B 1F DSP Program selection →USER Program
7 w 00 2C ⇒Page 44
8 w 01 00 Adaptive mode :Disable
9 w 01 04 Adaptive mode :Enable
10 w 00 00 ⇒Page 0
11 w 02 00 Standby Mode disable
12 w 03 00 LR Mute:Off
end
When started thereafter Step-5 of TAS5766M, it was the following movement.
(1) Even if Standby is disabled, a sound doesn't out.
(2) Even if 0x2B is returned to 01(Default), a sound doesn't out.
I think that the cause of (1) are no writing in CRAM.
Please let me know about cause and measure of(2).
Best regards,
Satoshi