Hi All,
I'm using two LME49740 IC's as panpot buffers in the bus assignment section of a mixing desk. This is the part where you decide if you send a mono signal to either the left or the right main summing bus (or odd or even subgroups) or to both to have the mono signal sent in equal amounts to left and right. It is a dual 4K7 linear pot that has 4K7 'pull up' resistors to the wipers (to make the centre attenuation 4.5 dB rather than 6dB). The wiper contacts go straight to the 4 non-inverting inputs of each LME49740 (one for left, and one for right). Each opamp channel's output is shorted to the inverting input, and the four output terminals are connected together via 10 Ohm resistors. The paralleling of four opamp sections is to get the output capacity to drive low impedance summing buses, and to also take advantage of the lower noise of parallel amplifier sections.
AC performance is fine and as expected, but something strange happens to the DC performance as the panpot nears the ends of its range. When panned centre, the output impedance of the panpot is just short of 1K and the outputs of each quad buffer is practically at 0V. When the panpot is all the way to one side, the outputs are at about -20mV (even though the input is at 0V, or at the -0.1mV offset of the opamp driving the panpot). With the panpot about 100 Ohms away from its extremes of travel, output offsets are fine again. Just as a sanity check, I swapped an LME49740 for the trusty old TLO74 and that behaved fine. Could this be anything to do with interaction of bias cancellation circuitry? Any ideas?
Just in case this was something to do with the paralleling of 4 opamp sections, on one of the LME49740's I isolated the input and the output so that it was only a single opamp channel being driven. The output offset reduced to -7mV but again disappeared when the panpot was not at the extremes of travel.
Has anyone else had this issue with the LME49740 as voltage follower, or am I doing something stupid somehow? My 100M scope doesn't detect any AC oscillation and each opamp is decoupled at the supply pins.
Many Thanks for any replies,
Bjorn