Hello,
I'm actually designing a amplifier based on the tas5630b chip.
I need to switch between one and two channels in btl mode. Most of the time I work just with one channel (A+B), so I need to shutdown the second (C+D) one to keep the switching losses low.
Is there a way to disable the second channel by a µC without having a failure on ready pin?
I thought about several possibilities:
- disabling the bootstrap fets with a fet, controlled by a µC
- shutting down PVDD with relay and µC
- shutting down GVDD with a analog switch and µC
I guess the best way is to shut down GVDD using a analog switch, controlled by µC. But I don't know if ready still stays high if I do so?
Can you please help me with this?
Thanks a lot.
Best regards
Bernhard Waechter