I'm using the TPA2006 Audio Amplifier and I've followed the datasheet recommendations but I'm having a problem with power supply noise getting through to the speaker audio. I'm getting no where near the -55dB as stated in the datasheet.
I'm using the amp in with a single ended input and my input resistors are set to 43.2kohm so I'm using a higher gain that unity. However, when I set my input resistors to 150kohm to set it to unity gain there is no change in the PSRR.
I'm using a 1uF cap placed close to the TPA2006 and I'm also using a 10uF cap close by as well.