Hi Ti Engineers.
I am evaluating the TAS5754M(EVM).
I have a question about IPVDD at Power down.
IPVDD described as 8~9mA on DATA sheet(SLAS987)
However it was 0.1~0.2mA when actually I measure.
Why such a difference occurs?
<Conditions>
Connection: 24V---<Ammeter>---Pin No.6 and No.7
PVDD: 24V
SPK_GAIN: 20dB
fSPK_AMP: 768kHz
Powerdown Request Register: [1] Powerdown mode
Best,Regards