Hi,
When TAS5614LA configures as mode [3:1] = 001 (1N+1/2xBTL/AD mode), how do I treat unused input pin such as INPUTB and INPUTD?
i.g. connect to GND via pull down resistor approx. 47kohm and so on...
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
When TAS5614LA configures as mode [3:1] = 001 (1N+1/2xBTL/AD mode), how do I treat unused input pin such as INPUTB and INPUTD?
i.g. connect to GND via pull down resistor approx. 47kohm and so on...
Regards,
Hello,
Yes that is correct you should tie the unused input to ground with either a pull down resistor or directly. (A pull down may offer more flexibility if rework is needed)
Best Regards,
Matt