Hi,
I am working on a project which requires a single-ended to differential converter driving ~3 meter of shielded twisted pair. The required (differential) gain is Vdiff = Vout(+) - Vout(-) = 2 * Vin. Input signal is -10V < Vin < +10V, and so are Vout(+) and Vout(-). (note that -20V < Vdiff < 20V). Required bandwidth is <1 MHz.
Based on these criteria I selected the following candidates: DRV134/135, LME49724, THS4130/4131
The DRV134/135 matches the bandwidth requirement and only requires a few external components. Downside is the relatively high input voltage noise density of 35 nV/rtHz.
The LME49724 and THS4130/4131 perform much better at 2.1 nV/rtHz and 1.3 nV/rtHz, but the bandwidth is much higher (50 / 150 MHz). To benefit from the lower noise density I have to reduce the bandwidth; for example by including a capacitor in each feedback path. I read everywhere that both feedback paths should be closely matched to not run into problems; but it seems impossible to get tight tolerances on capacitors.
Questions:
- Which part no. would you recommend for the application?
- Is it required to get matched capacitors? And if so, how do I select/match them?
- Anything to watch out for?
Thanks!